Honeywell Vector Space Sense

A Smarter Way to Manage Building Spaces and Make Every Square Foot Count

A building’s value is based on what it can provide an organization, and how its spaces can contribute to organizational outcomes. However, it can be tough to know exactly how building spaces are being used at any given time, and if they are being used to their full potential.​

The ramifications of not knowing the full extent of a building’s usage, or its underuse, are substantial. Empty office space is a silent expense for organizations, with large companies potentially overpaying millions of dollars each year for the space they do not use – yet lacking the insight to realize that this is occurring. 

That is where Honeywell Vector Space Sense can help.​​



Deeper Connections Enable Deeper Visibility

Leveraging the power of the Internet of Things (IoT), Honeywell Vector Space Sense shows exactly where, when, and how building spaces are used at any given time, presenting actionable insights for more informed decision-making around space usage. 

Based on a sensor-agnostic design and part of Honeywell’s broader Connected Services portfolio, Honeywell Vector Space Sense accesses data gathered by occupancy sensors installed anywhere within a building, from lighting to desks, that can help provide a more accurate picture of the actual utilization of the building and the individual spaces inside it. Analysis based on custom algorithms, followed by detailed, information-rich dashboards and utilization maps, provides visibility into usage that can inform space management and planning.​

Data Insights for Putting Building Spaces to Work​

With Honeywell Vector Space Sense, organizations can access more insights than ever before, such as:

  • Where spaces are being under-utilized, so organizations can repurpose them for more productive uses. 
  • Where spaces are being over-utilized, so organizations can regulate traffic to improve occupant experiences, and also prioritize housekeeping and maintenance schedules accordingly.
  • Actual building-occupancy patterns to inform appropriate building management system (BMS) schedules, instead of following fixed timings, which can help organizations improve overall system efficiency and energy savings.
  • Utilization trends to inform future space investments or divestments, as well as to help assess whether sufficient space is available at any given time to plan for pending headcount increases.

Confident Decision-Making for Measurable Impact​

Honeywell Vector Space Sense can contribute to an organization’s bottom line in significant ways. From helping organizations improve cost savings by estimating space change needs with greater precision, to providing information that can enable better occupant flow and usage patterns, to improving user experiences, Honeywell Vector Space Sense delivers connected, data-driven insights to inform changes that promote lasting, measurable results.

​​​​​​​​​​​​​